SPI - set inactive state of SOUT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI - set inactive state of SOUT

751 Views
vix
Contributor II

SPI on Vybrid can be configured through a dedicated set of registers.

Inactive state for PCS and SCK can be configured with PCSIS (in SPIx_MCR) and CPOL (in SPIx_CTARn).

I don't find a way to set the inactive state for SOUT, and with an oscilloscope I see that this is HIGH.

Is there a way to set it to LOW?

Tags (1)
0 Kudos
1 Reply

549 Views
art
NXP Employee
NXP Employee

There is no way of configuring the inactive state of the SOUT signal, it is always High.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos