Is there an application note (as AN2919) to determine I2C SCL frequency for P1010 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there an application note (as AN2919) to determine I2C SCL frequency for P1010 ?

421 Views
fabricedecrop
Contributor I

I need to set up FDR and DFSRR on my platform based on P1010. Is there an application note to help me ?

Thanks,

Fabrice DECROP

0 Kudos
1 Reply

350 Views
ufedor
NXP Employee
NXP Employee

The AN2919 is applicable for the P1010 - refer to the options for the P2020.

0 Kudos