KW40Z HardFault in hciLeCallback

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW40Z HardFault in hciLeCallback

694 Views
bpratt
Contributor I

Hello,

I am using the KW40Z in the GAP Central role to scan and connect to other BLE devices. Occasionally, a HardFault will be triggered while processing scan requests. I've managed to trace the issue back to a potential null-pointer dereference in "hciLeCallback" from "gap_hci_cb.o" in "ble_host_central_lib.a" within Connectivity Software 1.0.1.

The disassembly for this function is shown below. There is a conditional breakpoint on address 0x1875C right after the call to "MEM_BufferAlloc". Notice that there is no check to verify that "MEM_BufferAlloc" did not return NULL, unlike the previous call to "MEM_BufferAlloc" earlier in the function (starting at address 0x18736, the "MOVS" followed by the "BEQ.N").

pastedImage_1.png

Ultimately, the HardFault occurs within the call to "FLib_MemCpy" at address 0x1877C where we end up trying to write to address 0. A snapshot of this condition is shown below (destination in R0, source in R1). There are a few reads and writes that occur between the call to "MEM_BufferAlloc" and "FLib_MemCpy" that I haven't fully decoded, but they don't seem to help us avoid writing to address 0.

pastedImage_5.png

I suspect I can increase the heap size to avoid running into this situation, but it doesn't fix the underlying cause. Is there a planned update to the Connectivity Software that happens to address this issue?

Thanks,

Ben

Labels (1)
0 Kudos
2 Replies

429 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Ben Pratt

Thanks for your feedback, I will verify this information and tell to the people that take care of this. Your issue seams to be a improvement, so it should be in the next release, but it may take time to be released.

Best Regards

Jorge Alcala

0 Kudos

429 Views
bpratt
Contributor I

Hi Jorge, 

Thanks for the acknowledgement. Increasing the heap size did allow us to avoid the situation. Looking forward to the next release.

Thanks,

Ben

0 Kudos