ATMEL WIFI BLE ATWILC3000-MR110CA Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ATMEL WIFI BLE ATWILC3000-MR110CA Driver

1,439 Views
kunalbarot
Contributor I

I need software stack/driver of atmel wifi-ble module ATWILC3000. I need to interface this module to my NXP host processsor(NXP i.MX6UL 698MHz ARM A7)

Thanks

Tags (3)
0 Kudos
1 Reply

769 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Kunal Barot,

You would need to reach the manufacturer of  the module to obtain a driver, as this is not included on the i.MX6UL EVK.

There are some github that contains the driver or information for this module:

https://github.com/atwilc3000/driver

And they also have a driver ready to work in Yocto. I haven’t tried integrating it to the FSL Community BSP but you may see if it’s plausible.

https://github.com/atwilc3000/meta-wilc

I hope this helps!

Regards,

0 Kudos