AnsweredAssumed Answered

FRDM-MK66F - WHERE DO CAN 0 PTA12/13 or CAN 1 PTE24/25 PINS GO??

Question asked by Matthew Staben on Mar 3, 2017
Latest reply on Mar 6, 2017 by Matthew Staben

We are evaluating several micros to replace the erstwhile Luminary Stellaris LM3S9B96 (TI) part that suddenly went obsolete.  The NXP MK66FN2M0VLQ18 has been identified as a potential replacement that will be the base for a new Core board.  

 

For the board to be a viable candidate AT ALL, it must be CAN compatible with the processors that the MK66F will need to communicate with.

 

To do this, we want to confirm that the CAN module is in fact compatible with the other processors.  Unfortunately, I am unable to find any reference on the FRDM-K66F eval. board, or any schematic, that labels where the pins actually wind up on the etch so that I can breadboard a CAN transceiver and see if it can talk to the others.  Perhaps I am blind.

 

Regards,

Outcomes