libphp5.so not created in Yocto QorIQ-SDK-V2.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

libphp5.so not created in Yocto QorIQ-SDK-V2.0

508 Views
sangavip
Contributor I

I cross compiled apache2 and php for t2080rdb-64b(PowerPC) in yocto QorIQ-SDK-V2.0 in X-86-64bit system(Ubuntu). But the libphp5.so for the target board was not created during cross compilation. I couldn't figure out what is the error. It will be very helpful if someone clarifies my doubt. Thanks in advance.

Tags (1)
0 Kudos
1 Reply

292 Views
alexander_yakov
NXP Employee
NXP Employee

Googling by "libphp5.so cross compile", I see the problem is related to apache. For example:

php - libphp5.so not being created after compiling and prefix directory not created - Stack Overflow 


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos