IMX7 ADC question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX7 ADC question

Jump to solution
888 Views
frankyhsu
Contributor III

Hi

I am checking the ADC input resistance for IMX7 and I found the R_IEXT need to be small to driver the ADC input. Does it mean we need to have 50~250 ohm pull-high to 1.8V and use 10k NTC to GND? Like the below schematic?

pastedImage_3.png

Franky

Labels (1)
0 Kudos
1 Solution
502 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Franky,

Such parameter is not specifically about such hardware configuration (although the idea is maintaining the impedance as low as possible). However, you could refer to the following documents/application notes about ADC parameters and recommendations:

http://www.nxp.com/assets/documents/data/en/application-notes/AN2438.pdf

http://www.nxp.com/assets/documents/data/en/application-notes/AN1058.pdf

http://www.nxp.com/assets/documents/data/en/application-notes/AN4373.pdf

 http://www.nxp.com/assets/documents/data/en/supporting-information/Analog-to-digital-Converter-Train...

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
503 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Franky,

Such parameter is not specifically about such hardware configuration (although the idea is maintaining the impedance as low as possible). However, you could refer to the following documents/application notes about ADC parameters and recommendations:

http://www.nxp.com/assets/documents/data/en/application-notes/AN2438.pdf

http://www.nxp.com/assets/documents/data/en/application-notes/AN1058.pdf

http://www.nxp.com/assets/documents/data/en/application-notes/AN4373.pdf

 http://www.nxp.com/assets/documents/data/en/supporting-information/Analog-to-digital-Converter-Train...

Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------