Question, i.MX6DualLite/ ARM errata#782773

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6DualLite/ ARM errata#782773

575 Views
SLICE
Contributor IV

Dear team,

I would like to ask about a workaround of ARM errata #782773(mentioned as ERR005386 of i.MX6DL errata).

My customer is trying to implement the workaround for the ARM errata#782773 into their software.

Their software is based on your LinuxBSP(L3.0.35_3.0.0-rc4), and they think the workaround is not implemented in your original LinuxBSP.

Is it true?

Thanks,

Miyamoto

0 Kudos
1 Reply

404 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

yes, true. It was discussed previously internally with below summary:

After looking at the thread below:

http://lists.infradead.org/pipermail/linux-arm-kernel/2012-September/123101.html

ARM thinks this should not errata will not occur in Linux, apart from a remote possibility of failure during boot.
BSP team do not see any other references to this errata in Linux code base.
Customer can add the workaround if they feel they are updating page tables

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos