AnsweredAssumed Answered

What is the recommendation when using JTAG boundary scan but not using PCIe on iMX7 ?

Question asked by John Watlington on Feb 27, 2017
Latest reply on Sep 19, 2017 by ulrik kristiansen

We are using an iMX7 Dual SoC, and while we appreciate the inclusion of a PCIe interface we currently have no use for it in our design.  In Section 3.2 of the datasheet (iMX7Dual Family of Applications Processors Datasheet, Rev. 2, 06/2016), Table 5 recommends that if not using PCIe to leave a number of signals floating, and to tie PCIE_VP, PCIE_VP_RX, PCIE_VP_TX, PCIE_VPH, PCIE_VPH_RX, PCIE_VPH_TX, and PCIE_REXT to ground.

 

In Table 8 of the hardware development guide (Hardware Development Guide for i.MX7Dual and 7Solo Applications Processors, Rev. 0, 07/2016), note 5 says that if JTAG boundary scan is to be supported, the following supplies must be powered: PCIE_VP, PCIE_VPH, PCIE_VP_TX (the doc has a typo on that last signal name).

 

The question is, in the case of not using PCIe, but desiring to support boundary scan, exactly what should all the other pins be connected to ?

 

The literal interpretation of the documentation results in:

PCIE_VP  powered by LDO_1P0D

PCIE_VP_RX tied to ground

PCIE_VP_TX powered by LDO_1P0D

PCIE_VPH powered by VDDA_PHY_1P8

PCIE_VPH_RX tied to ground

PCIE_VPH_TX tied to ground

PCIE_REXT tied to ground

 

Is this correct ?

 

I'm assuming that since PCIE_VP, PCIE_VPH, and PCI_VP_TX are only used for infrequent JTAG, it is OK to only provide the internal LDO_1P0D regulator with minimal bypassing (0.22uF), and supply the PCIE_VPH supply from the +1.8V switch (VDDA_PHY_1P8) without bypassing.   MIDI is also powered down via the instructions in Table 5 of the datasheet.  Comments ?

Outcomes