I'm using the FRDM-KL03Z evaluation board with kds. Where can I find the TPM_BWR_xxx definitions? I don't want to use the predefined functions to control the timers, I want to write to the registers directly. Are there any good references around for this microcontroller?
Thanks!
Solved! Go to Solution.
Hi
Maybe you can use the MKL03Z4.h in SDK_2.0_FRDM-KL03Z.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
Maybe you can use the MKL03Z4.h in SDK_2.0_FRDM-KL03Z.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Robin,
Thanks for pointing me in the right direction. I now have another question! When I look through the definitions in that file, I see that there are read (RD) and write (WR) operations as well as BRD and BWR. What does the “B” mean? When should I use the RD versus the BRD and same for the WR and BWR?
Thanks,
Sara
Sara Stout-Grandy, M.Eng., Ph.D., P.Eng.
Senior Hardware Designer
20 Angus Morton Dr., Bedford,
NS, Canada, B4B 0L9
902-450-1700, x278