AnsweredAssumed Answered

Ethernet crash LS1021A TWR

Question asked by AMOL SHROTRI on Feb 27, 2017
Latest reply on Mar 6, 2017 by AMOL SHROTRI

Hello,

 

I am trying customized bootload to boot linux on LS1021A rev2 board. We could boot the board and launch the Linux kernel. But I am facing issue while accessing ethernet interface, it gives kernel crash.

1. When i execute command #> udhcp eth2 

2. Instead of dhcp i tried to set staic IP and ping localhost it works fine but when try to ping remote IP gets same kernel crash.

 

udhcpc: started, v1.25.1
udhcpc: sending discover
udhcpc: sending discover
fsl-gianfar soc:ethernet@2d90000 eth2: Link is Up - 1Gbps/Full - flow control rx/tx
udhcpc: sending discover
udhcpc: sending discover
udhcpc: sending discover
------------[ cut here ]------------
WARNING: CPU: 0 PID: 0 at net/sched/sch_generic.c:318 dev_watchdog+0x159/0x1bc()
NETDEV WATCHDOG: eth2 (fsl-gianfar): transmit queue 0 timed out
Modules linked in:
CPU: 0 PID: 0 Comm: swapper/0 Not tainted 4.1.8-rt8 #24
Hardware name: Freescale LS1021A
[<8001b74d>] (unwind_backtrace) from [<80018d5d>] (show_stack+0x11/0x12)
[<80018d5d>] (show_stack) from [<803acb1d>] (dump_stack+0x51/0x64)
[<803acb1d>] (dump_stack) from [<80025f37>] (warn_slowpath_common+0x63/0x88)
[<80025f37>] (warn_slowpath_common) from [<80025f7d>] (warn_slowpath_fmt+0x21/0x2a)
[<80025f7d>] (warn_slowpath_fmt) from [<8033e9ad>] (dev_watchdog+0x159/0x1bc)
[<8033e9ad>] (dev_watchdog) from [<800583e9>] (call_timer_fn+0x43/0xb2)
[<800583e9>] (call_timer_fn) from [<800588db>] (run_timer_softirq+0x16f/0x1a4)
[<800588db>] (run_timer_softirq) from [<8002889d>] (__do_softirq+0xd1/0x1c8)
[<8002889d>] (__do_softirq) from [<80028de9>] (irq_exit+0x51/0xa0)
[<80028de9>] (irq_exit) from [<8004e215>] (__handle_domain_irq+0x5d/0x7c)
[<8004e215>] (__handle_domain_irq) from [<80009281>] (gic_handle_irq+0x2d/0x44)
[<80009281>] (gic_handle_irq) from [<803b005b>] (__irq_svc+0x3b/0x5c)
Exception stack(0x80bddf58 to 0x80bddfa0)
df40:                                                       00000001 00000000
df60: 00000000 80022041 80bdc000 00000000 80bddfa8 803b5abc 00000000 00000001
df80: 805f3410 00000000 80bde180 80bddfa0 80016deb 80016dec 400d0033 ffffffff
[<803b005b>] (__irq_svc) from [<80016dec>] (arch_cpu_idle+0x1a/0x26)
[<80016dec>] (arch_cpu_idle) from [<800487d3>] (cpu_startup_entry+0x1db/0x218)
[<800487d3>] (cpu_startup_entry) from [<805bf91f>] (start_kernel+0x27b/0x2e4)
---[ end trace 7ca9e3f44035910c ]---
fsl-gianfar soc:ethernet@2d90000 eth2: Link is Up - 1Gbps/Full - flow control rx/tx
udhcpc: no lease, failing
FAIL
From bootloader, I even configuring below registers as
1. SCFG_ETSECDMAMCR = 0xf800120f
2. SCFG_ETSECCMCR = 0x4000000

 

Do I need to add any additional configuration in bootloader before launching kernel?

 

Thanks & Regards,

Amol M Shrotri

Outcomes