Dear support team,
We are using imx6Q custom platform based on sabresd platform for our development with Linux 3.10.17_1.0.0-GA BSP.
We would like to use a 20-bit parallel camera input through CSI0.
Please let us know, will the CSI0 support 1920x1080P @60fps?
Thanks and Regards,
Ansari
Hi Ansari
yes it supports, CSI IPU performance is described in sect.37.1.2.1.1 Camera Ports i.MX6DQ RM
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
For parallel interface, the maximum speed of the interface is 240Mhz.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------