Hi ,
I prepared yocto images according the imx-yocto user guide , but while booting the UART debug is showing nothing.
while porting we used sdcard .
I used dd command to put images into the sdcard.
Kindly help immediately.
Thanks in advance.
Thanks and Regards
Abhirup Mitra
Hi Abhirup Mitra,
-Verify that the serial connections is working fine, please try first with a different device to be sure that serial communication is not the problem.
- After flashing the image in the SD card remove it and insert it again in the PC. Then verify that the 2 partitions are created succesfully. In one partition you must have zImage and .dtb file. In the other you must see the Linuxw file system.
- Double check that the switches are configured to boot from SD card.
- If the problem persists please send the list of commands you used to build and deploy the image? I need to know the exact commands you used to verify if the process was correct.
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------