- I have problem with the pinmux regarding eSPI1_ss0 . when i try to configure the pin mux to ALT0 at IOMUXC_SW_MUX_CTL_PAD_KEY_ROW1 the interfaces doesn't work properly. while using ALT5 which seems to be the default the interface works.
1.What is the meaning of the "RESET" line the register figure on 36.4.125 figure ?
2. how to confige eSPI1_ss0 to work with ALT0 and not ALT5?
Regards,
Barak
Hi Barak
seems driver linux/drivers/spi/spi-imx.c uses only alt5 option, "cs-gpios".
"RESET" line means register values after reset.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Do you have \ Can you send me a driver version that uses "slave select" , ATL0 ?
Do you have \ Can you send me a driver version that uses "slave select" , ATL0 ?