AnsweredAssumed Answered

CCA Features in Generic FSK mode on KW41Z

Question asked by Sam Petersen on Feb 23, 2017
Latest reply on Feb 26, 2017 by Bill Krakar

Is it possible to perform some sort of clear channel assessment when using the Kinetis KW41Z in Generic FSK mode? I'm trying to implement a custom MAC layer that uses CSMA, but the example code and genfsk libraries don't expose any type of CCA or ED features as far as I can tell. There are support functions for performing CCA/ED in the 802.15.4 library, but I don't think I can use them with Generic FSK - my attempts so far have been unsuccessful.

Outcomes