AnsweredAssumed Answered

usb debugging problem in Imx6 sabre board

Question asked by sameerarvikar on Feb 23, 2017
Latest reply on Dec 5, 2017 by Benson Wu

I am trying to use adb commands with the board , Its having kitkat installed on it

 

Now the problem is that usb debugging port (otg port ) in imx6 sabre board is also used for putting input devices (like mouse and keyboard)

So i enable usb debugging option in android using mouse

 

Now when i connect usb debugging using the cable with computer , the android asks for (allow device to connect on its display) , but because i have no option for input device like a mouse (as the port is busy ) so i can never allow the device to connect. and hence adb devices command output is always 

 

Device id  ---   unauthorised

 

So what is the solution or workaround of this problem ??

Outcomes