S32 Design Studio include path

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio include path

6,913 Views
qiaodeng
Contributor II

Hi,

 I want to link some other files into my project, where should I add the file path ?

I have add the path here ,but it does not work.

 

Best Regards

Qiao

Labels (2)
0 Kudos
8 Replies

4,161 Views
stanish
NXP Employee
NXP Employee

Hi,

Include paths are intended for header files only.

If you have external library you can add the path into linker:

pastedImage_2.png

In case of any other file/object:

pastedImage_3.png

This is how the settings above influence the .arg file used by makefile:

"./Project_Settings/Startup_Code/system_S32K144.o"
"./Project_Settings/Startup_Code/startup_S32K144.o"
"./Project_Settings/Startup_Code/startup.o"
"./src/main.o"
-L:My_External_lib.a
-T
"C:/Users/r200040/workspaceS32DS.ARM_1.3/S32K144_Segger_test/Project_Settings/Linker_Files/S32K1xx_flash.ld"
-Wl,-Map,"S32K144_Segger_test.map"
-Xlinker
--gc-sections
-mcpu=cortex-m4
-mthumb
-specs=ewl_c9x_noio.specs
--sysroot="C:/NXP/S32DS_ARM_v1.3/S32DS/arm_ewl2"
"Any_other_file.bin"
-lc:\MyLib

Regarding the elf question please have a look here:

https://community.nxp.com/docs/DOC-332252 

Hope it helps.

Stan

0 Kudos

4,076 Views
rathi_tg
Contributor III

 

Hello @stanish 

My Project does not have option such as  C/C+Builder its an Matlab XML Impoerted Project.

rathi_tg_0-1601715380729.png

 

 

Could you guide me the way to resolve it.

Regards 

Gopal Rathi

0 Kudos

4,162 Views
martin_kovar
NXP Employee
NXP Employee

Hello Qiao,

I am not definitely sure, but I think it is not possible to add path to file directly in S32DS. You have to edit the .args file in your project. But be careful, .args is automatically generated by S32DS when you compile the project. 

So at first, compile the project and then edit the .args file. If you do it in opposite way, S32DS will delete your changes.

My colleague solved very similar problem in the following thread. Please look:

https://community.nxp.com/thread/445212 

If you have any other questions, please feel free to write me back.

Regards,

Martin

0 Kudos

4,162 Views
michaelchien
Contributor II

Hello Martin

    According to your reply" it is not possible to add path to file directly in S32DS". If there is a file OBCM.c in app folder and main.c in src folder, I can't inlcude the OBCM.c file in main.c such as  writing #include "OBCM.c" in the top of main.c ?

0 Kudos

4,162 Views
stanish
NXP Employee
NXP Employee

Hi Michael,

Yes, you could be able to include OBCM.c file but you should add the include path in the project properties.

Nevertheless including ".c" files is not a good coding practice and could introduce some hard-to-find problems to your project.

Stan

0 Kudos

4,162 Views
michaelchien
Contributor II

hi Stanislav

        I follow your suggestion and the error message" can't find out the .h" is disappeared when I add the path in the  C complier Includessetting . It seems to be able to recognize the .h file. But it shows another error, " undefine reference to my_function() which I have defined in my h file, extern void my_function(void).  Do you have any idea for this? Thank you!

0 Kudos

4,161 Views
qiaodeng
Contributor II

Hi Martin,

    Here is another question. I want to compile the code using some other compiler, and then import the elf file into S32 Studio to flash my MCU. Is it supported by S32 Design Studio? How should I do it.

Regards,

Qiao

0 Kudos

4,162 Views
stanish
NXP Employee
NXP Employee

Hello Qiao,

Yes this is possible. Please have a look here:

https://community.nxp.com/docs/DOC-332252 

Note:

We've experienced some limitations with debugging elf built with GHS build tools + GDB .

Stan

0 Kudos