AnsweredAssumed Answered

LPC-Link + LabTool with external RAM and data streaming via Wi-Fi

Question asked by HM Yoong on Feb 22, 2017
Latest reply on Feb 23, 2017 by jeremyzhou

I would like to use LPC-Link2 and LabTool to sample analog data up to 80 Msps for 0.1 and transfer the data remotely via ESP8266 or other Wi-Fi transceiver.  LPC4370 only has 282 kB RAM.  Doing the maths and with the non-deterministic nature of TCP/IP, is there a better to do it? I do not have the expertise and time to develop my own boards with external SDRAM and required hardware from LabTool. Thanks.

Outcomes