Hello,
I just wonder how to make PWM signal that much higher than 1/255 resolution.
it is mentioned in the datasheet, PWM duty cycle = [ (PWMPER - PWMDTY) / PWMPER ] * 100%
but both of the register value is 8-bits sized, so that the max duty resolution can be 1/255.
I need to control at least 0.1% of duty or more. do you have any idea?
Hi Daehyeon,
MJW is right. You should concatenate two 8bit PWM counters into one 16bit.
Example of 16bit PWM initialization:
//==============================================================================
// PWM_Init
//==============================================================================
void PWM0_Init(void)
{
//8MHz bus clock
//for example we want to generate initial PWM wave on PWM01 channel 1kHz with 50% duty cycle
//two 8bit channels 6 and 7 are concatenated to one 16bit channel
PWM0POL = 0xC0; //polarity - PWM channel 67 is high at the beginning of period, then low
PWM0CLK = 0x00; //select clock source A for channel 6-7
PWM0PRCLK = 0x01; //prescaler for clock A -> BusClock/2 = 8MHz/2 = 4MHz
PWM0CAE = 0x00; //channel 67 operate in left aligned output mode
PWM0CTL = 0x8C; //we use 16bit PWM 67, disable clock in wait and freeze mode
PWM0CNT67 = 0x0000;//reset the counter of PWM67
PWM0PER67 = 4000; //PWMPER67 = clock / PWM7frek = 4000000 / 1000 = 4000
PWM0DTY67 = PWMPER67/2; //ensure duty cycle 50%
PWM0E = 0x80; //enable PWM67
}
Per RM, the S12ZVC contain two 4-channel 16-bit PWM modules - PWM0 gated from bus clock and PWM1 gated from core clock.
In fact, both modules are 8-channel 8-bit PWM modules, but only odd channels are routed to the external pins. Therefore, we may use only 4 channels from each module configured either as 8bit or 16bit.
I hope it helps you.
Have a great day,
Radek
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
you can concatenate two 8-bit PWM channels into one 16-bit channel.
Please refer to the description of PWMCTL (specifically: the CONxx fields) in the RM for details.
HTH,
MJW