Hello,
In following community thread, BT656 output patch for i.MX6 were released.
And newest one is support 2x video output for BT656 and LVDS output.
Our customer plan to use 2x output, 800x480 WVGA LCD and bt656 VGA.
For example. Pixel clock of each video out must be divisible from same number
because it must use same PLL output.
Best regards,
Ishii.
Hi
Thank you for your reply.
And sorry for my less information.
Current community thread is a following.
https://community.nxp.com/docs/DOC-94019
Best regards,
Ishii.
yes, I think so, if you need to use mxcfb1, thy to set in the uboot command.
for restriction, ipu can support up to 240M. for pixel clock set, you can refer to the patch and source code in the bsp.
which community thread do you mean? pls post again, thanks.