Transfer data from PC to Android via NFC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Transfer data from PC to Android via NFC

748 Views
alibigdeli
Contributor I

NFC   I  need to send some screen shots from my PC to my android device via NFC tags. How is that possible?

Thanks

Tags (1)
0 Kudos
1 Reply

519 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Bigdeli ,

The solution is possible, but not good, because RF transmitting speed is only 106Kbps. One of the 2 ways can be used :

(1) NFC reader is required on PC board.

(2) NFC reader module can be connected to PC USB

NFC reader IC can be NCP3000 or PN7150.

Actually, your solution can also use WIFI to transmit image data between PC & android device!

Regards,

Weidong

0 Kudos