RAJIV BANDODKAR

Stabilization capacitor for S12ZVL32 Regulator

Discussion created by RAJIV BANDODKAR on Feb 16, 2017
Latest reply on Feb 23, 2017 by Daniel Martynek

Hi,

Wondering if the recommended stabilization Capacitor can be reduced (minimum 4.7uF is recommended). My application using S12ZVL32 is running at 25MHz with internal oscillator, without external ballast transistor and an external load of around 20mA max. Application uses LIN Phy (+SCI), ADC, RTI, API, HVI and Timers. I am already using a 1uF ceramic capacitor across Vdda and Vddx pins, so around 2uF near the MCU.

Please comment..

Attachments

Outcomes