AnsweredAssumed Answered

USB-KW24D512 system reset will cause USB CDC module reset as well

Question asked by Xiao Ma on Feb 15, 2017
Latest reply on Feb 21, 2017 by Xiao Ma

Hi,

I'm using USB CDC Driver of USB-KW24D512 Dongle as a virtual com port on Windows OS. I can use Putty to communicate with the USB Dongle.

 

One requirement for me now is that when the MCU occurs a software reset (for example, set the SYSRESETREQ bit), I would like not to reset USB CDC module. If so, I need to restart the putty to connect with the device again. This is doable for manual configuration, however, that would not be a good way for automation software.

 

Therefore, is there a way to bypass the USB CDC module reset when a system reset occurs or is there a kind of Reset which only erases the RAM memory?

 

Thanks for any help.

Outcomes