AnsweredAssumed Answered

JN5168 coordinator network to control third party end devices

Question asked by Jaffin MK on Feb 14, 2017
Latest reply on May 27, 2018 by Patrick Pan

Hello

 

I just started with zigbee development with jn5168 module. After few playing around, I wanted to make the module into coordinator and connect philips hue bulb to it. I had downloaded the JN-AN-1223-ZigBee-IoT-Gateway-Control-Bridge-v1008 application note. I flashed the coordinator firmware into the jn5168 module and tested it with TestGUI.exe. I had followed intructions in the application note document. And formed the zigbee network. Then I tried to connect the bulb by clicking permit join with parameters FFFC and FE(address mode and time interval). The permit join status is TRUE. But the hue bulb doesnt connect. I am very confused. Because at this moment I should be able to connect to it. 

 

How can I find out the address of the bulb and connect directly? Is there an option to reset the bulb with the jn5168 bridge coordinator. 

Right now I am only following this particular application note. Please advise if there is anything more that should be done for the connection.

Outcomes