Hi All
I am setting up a PE ADC High level component and am having a problem with the Internal Trigger, Trigger Input settings. This is for a 56F82748 DSC and using the 12 Bit Cyclic ADC.
I get the following error in the setttings.
and in the Problems it shows the following Errors.
The strange thing is that the ADC_LDD driver that the ADC High level component uses is happy...
... and it is set to the same TA0_OUT.
The error message seems to indicate that the XBAR is not set up properly. So I added it and the "Automatic" settings show that the timer I am using is routed to the ADC.
To me this seems like a bug but maybe I missed something.
Thanks for your Help!
Pete