Wich is the best choice for imx7d, MT29TZZZ8D5JKEZB-107 W.95Q or MT29TZZZ8D5JKEPD-107 W.95T?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wich is the best choice for imx7d, MT29TZZZ8D5JKEZB-107 W.95Q or MT29TZZZ8D5JKEPD-107 W.95T?

445 Views
noeliascotti80
Contributor I

Can you help me to find the best memory for my imx7d board?

The memory has to accomplish these requirements:

- 7 years longevity

- 0.5 pitch

- emmc memory integrated

- easy to get in small amounts

Tags (2)
0 Kudos
1 Reply

334 Views
igorpadykov
NXP Employee
NXP Employee

Hi Noelia

seems both can be used, for differencies one can ask micron.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos