AnsweredAssumed Answered

imx6q pinmux

Question asked by Angelo Dureghello on Feb 7, 2017
Latest reply on Feb 8, 2017 by igorpadykov

Hi, have some questions:

 

1) is setting of HYS and IBE bits enough to change pin direction into input ? From the pinmux port diagram, since the output

is connected to the input, any other bit needs to be set for the output part to be disabled ?

2) what happen to gpio output levels, when set to high, after cpu enters stop (deep-sleep) mode ? Levels are maintained ?

 

thanks

angleo

Outcomes