AnsweredAssumed Answered

Getting patch number / information from source?

Question asked by RY on Feb 6, 2017
Latest reply on Feb 7, 2017 by Daniel Chen

Is there an MQX version or string somewhere which shows/ keeps track of the patch number ?

 

I found MQX has  _mqx_version_number = 0x04020000; which is matched by string const _mqx_version = "4.2.0".

But it doesn't seem to account for patches.

E.g. the two patch archives that were released are 4.2.0.1 and 4.2.0.2. But after I have applied them, the mqx version number and the string stayed same. It seems the patches *should* (or not?) bump the last version byte, but they don't.

Outcomes