There is a function _tad_lightweight_memory_blocks, which prints information about the LWMEM blocks free and allocated on the system. But this only works if you built the system with lightweight memory management.
Is there similar function to the print memory information when not using LWMEM, when only MQX_USE_MEM 1 is defined?
Hi D.RY
When not using LWSEM, and define MQX_USE_MEM , we can get the MQX memory blocks info with TAD.
I tried this with Codewarrior.
Regards
Daniel
Hi,
Well that is with Code Warrior, I dont' know how it gets the numbers but I'm not using Code Warrior.
The code of the function I'm referring to uses LWMEM API, it won't even build without LWMEM support.
(Also you have a weird number on your screenshot above: -2141006748% ??)