Can LS1046a in EP mode act as PCIe bridge?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can LS1046a in EP mode act as PCIe bridge?

675 Views
sabine_s
Contributor III

That is, if the PCIe controllers are set up as 1 upstream and 2 downstream ports, can the PCIe controllers be configured so that transactions from the upstream port are routed to the proper downstream port (or local addressing space) and that transactions from a downstream port can be routed to either the upstream port, the other downstream port or local addressing space?

Another way to ask this might be: when an inbound transaction is received by a PCIe controller, the address is translated to a platform address. Is that translated address matched against all possible platform address destinations, including the PCIe controller outbound address windows?

Labels (1)
0 Kudos
1 Reply

550 Views
ufedor
NXP Employee
NXP Employee

There are no upstream and downstream ports in the LS1046A - i.e. it can't be mimic to a PCIe switch.

Please create a Technical Case to obtain details of the LS1046A PCIe streaming capabilities:

https://community.freescale.com/thread/381898

0 Kudos