The function of SNVS_LPCR register in i.MX6SX

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The function of SNVS_LPCR register in i.MX6SX

Jump to solution
626 Views
ko-hey
Senior Contributor II

Hi all

Please tell me the following registers function.

pastedImage_4.png

I want to control power ON/OFF by SW in i.MX6SX.

I understand it can power off by DP_EN and TOP fields from following thread.

i.MX6 SNVS_LPCR register and power down 

However, I can't understand how to power on by SW.

 

According to the RM, it seems that it can be power on by PK_OVERRIDE or PK_EN.

Can user power on by those bit ?

Also could you tell me the function of PK_OVERRIDE and PK_EN ?

Ko-hey

Labels (4)
0 Kudos
1 Solution
502 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

For i.MX6SX  SNVS[PK_OVERRIDE],  SNVS[PK_EN] are not supported

there is internal ticket get the RM updated accordingly.

Best regards
igor
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
503 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

For i.MX6SX  SNVS[PK_OVERRIDE],  SNVS[PK_EN] are not supported

there is internal ticket get the RM updated accordingly.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos