My company received two S32V234-EVB boards from NXP but they don't appear to have any linux OS or even uboot on them. The best I could do is get partial serial communication working over the micro USB connector using 38400,7,E,1 baud settings. Are there any prebuilt Linux images that I could flash on to an SD card to boot the board?
Thanks
Michael
NXP provides a Linux-based SDK for S32V development boards. The package installs on a Linux PC and can build binaries for your board from verified sources and with a verified toolchian/configuration. Please contact your distributor to obtain the package.
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Just checked what is actually available, there _are_ pre-built binaries, so you even to no t have to built them
on your machine. Just contact your distributor to help you to access the download page.
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------