Want MC9s08JM60 + SPI EE_PROM to appear as a disk-drive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Want MC9s08JM60 + SPI EE_PROM to appear as a disk-drive

772 Views
kim_a
Contributor I

The design is a configuration tool intended to change parameters in other devices. It should be possible to load a number of parameter files to the configuration tool from a PC and it would be preferred if the configuration-tool appear as a removable disk drive when attached to a PC-USB port. The hw involved is a MC9S08JM60 with a EE-PROM attached to the SPI port. Any easy way to do this ?

Labels (1)
0 Kudos
1 Reply

256 Views
JimDon
Senior Contributor III
What you want is the "badge board" bootloader source code.
At this years FTF they had a badge with a JM60 on it that you could program. When you connected the badge board to a USB part it came up as a hard drive and you could drop an s19 file on it for it to program.

You can get the source code from "canyourbadgedothis.com". You have to register then click "Contest Tools" and down load the Boot Loader zip file,. You will need CW 6.2 to build it.

I have not looked at yet, so tell us how it works out.

0 Kudos