AnsweredAssumed Answered

NAND Implementation for IMX536

Question asked by Leonardo Santos on Feb 2, 2017
Latest reply on Feb 8, 2017 by Leonardo Santos

Hello,

 

I am working on a imx53_loco based board and my last modification was to boot  the system through a NAND Flash memory. All parts of the system (hardware, bootloader, kernel and rootfs) are correctly settled-up and are working seamless (No "dmesg" prints indicating read/write errors, Read/Write from all the system components alike).

 

However, i don't know how to ensure the system is correctly adjusted and even if it will recover bad bits and set as "bad blocks" erroneous blocks of memory.

 

My first thought was to change the read function in NAND driver and randomly replace a bit in the page read to force the system to recover the information. Still, it doesn't cover the write process and i don't think that's the best practice for testing NAND operation.

 

I would be glad if anyone could help by suggesting some method, hardware or software for test the NAND operation and configuration in the hole system.

 

Some information:

Based on IMX53 loco board

fsl-community-bsp v1.8

 

Best regards,

Leonardo Ramos dos Santos

Outcomes