How to download a xxx.elf to my board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to download a xxx.elf to my board?

1,234 Views
xiexiaopeng
Contributor II

HI :

I'm a newcomer.

I'm working with MPC5775K now.

Now I have a xxx.elf ,how can I download it to my board,if I use the S32 Design Studio IDE.

Thank you!

Regards,

xie

Labels (1)
Tags (2)
4 Replies

952 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

you have to use some debug probe or stand alone Programmer. I recommend you to buy Universal Multilink FX, which is compatible with S32 Design Studio:

Universal Multilink FX High-Speed Development Interface|NXP 

Regards,

Martin

0 Kudos

952 Views
xiexiaopeng
Contributor II

Thanks Martin.

I have a Universal Multilink FX,I can download this elf to my board with the program, my question is I only have a xxx.elf and I have many board,how can I dowdload it to those board quickly.

what is the way can achieve my requirements.

Regards,

xie

0 Kudos

952 Views
martin_kovar
NXP Employee
NXP Employee

Hello Xie,

if you have only .elf file, you can use the tutorial I have created.

How to download separate .elf file to microcontroller using S32 Design Studio 

But if you have many boards, it will take some time. For this purpose, it is better to use standalone flash programmer. Please see following link:

P&E Microcomputer Systems: Over 30 years as an Industry leader in Embedded Systems Development Tools... 

If you have any other questions, please feel free to write me back.

Regards,

Martin

952 Views
xiexiaopeng
Contributor II

Thanks Martin,The method is best,I can download the .elf to my board. 

Thank you for your recommend ,I will use the standalone flash programmer.

0 Kudos