AnsweredAssumed Answered

Generating waveforms

Question asked by Martin Dusek on Jan 31, 2017
Latest reply on Feb 3, 2017 by xiangjun.rong

Hi,

is it possible to generate 24 MHz and 6 MHz signals (50% duty and in phase) with 12 MHz signal with shifted phase and reduced duty somehow using Kinetis microcontroller? Preferably with min. count of timer modules as we need one or two timer modules to be used for another purpose than generating this waveform?

 

Please see image.

Attachments

Outcomes