Sabre SD Eval Board - Maximum Total Size of MicroSD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sabre SD Eval Board - Maximum Total Size of MicroSD

468 Views
thomasmorrison
Contributor I

What is the maximum size the supported uboot/linux currently supports and what types

Does the Sabre board SDHS or SDXS?

I am investigating and I have  heard from our distributor that there are issues with some boards?

Tags (2)
0 Kudos
1 Reply

384 Views
Carlos_Musich
NXP Employee
NXP Employee

Hi Thomas,

What Sabre SD are you using of all?

If you are using IMX6QSABRESD you can find in IMX6Q Reference Manual that uSDHC module conforms to the SD Host Controller Standard Specification version 3.0, so you may check the spec to find out this information.

I am not sure, but I think the theoretical value is 2TB.


Regards,
Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos