What are LS-1021A SPI and HDLC maximum clocks (data rates)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What are LS-1021A SPI and HDLC maximum clocks (data rates)?

Jump to solution
682 Views
nxp_serge81
Contributor II

Hi. In LS-1021A datasheet it is said that for SPI min clk period is TPlat*8. What is TPlat? What is the top data rate of HDLC interface?

Tags (1)
0 Kudos
1 Solution
603 Views
nxp_serge81
Contributor II
0 Kudos
2 Replies
604 Views
nxp_serge81
Contributor II

Thanks a lot.

0 Kudos
603 Views
r8070z
NXP Employee
NXP Employee

Have a great day,

See Figure “Clock subsystem block diagram” in the LS1021A reference manual (chapter 4). There is Platform PLL which multiplies SYSCLK and provides platform clock. It should be in range 250 – 300 MHz. TPlat is platform clock cycle duration. Platform clock is applied to the SPI controller and to the QUICC Engine.

The TDM hardware maximum frequency is 50 MHz. This device supports TDM in a high-speed mode. To run in this mode, the QUICC Engine platform to TDM interface frequency ratio should be at least 8:1. For the ISDN protocol, the QUICC Engine platform to ISDN interface frequency ratio should be at least 16:1.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos