LS1043A Debug port in UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A Debug port in UART

535 Views
logeshs
Contributor II

Hi,

We are    LS1043A in our design, can you please confirm shall we use UART2 as the Debug port? we have connected UART1 with Network Switch.

Thanks

0 Kudos
2 Replies

383 Views
Pavel
NXP Employee
NXP Employee

Look at the Section 2.3.1 of the LS1043ARDB Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1043ARDBRM&Parent_nodeId=1441121579998719223109&Parent...

 

This Section contains instruction for using UART2 as terminal.

 
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

383 Views
logeshs
Contributor II

Thanks for your reply. So we can use any of the UART port as Debug terminal. 

Also in the Debug port we are using CTS and RTS pins and UART which connected to Switch does not use CTS and RTS.  If that is the case i hope we shall not configure the CTS and RTS of UART  which is connected to Switch as GPIO. Please confirm my understanding.

0 Kudos