AnsweredAssumed Answered

Is there a way to set up 2 processors on the same project?

Question asked by Becher on Jan 24, 2017
Latest reply on Jan 28, 2017 by SCOTT MILLER

I am using a MC56F82746 in a project but have an EVM with a MC56F82748 on it.  I want to do preliminary coding on the EVM and then easily switch it to the production board using the other processor.

I can add a second processor to the PE project but when I switch between them it comes up with the following message.

Is there a way to do this without loosing configuration for a processor?

Is the problem just for the Pins1 component?

Is there a better way to do this?

Thanks

Pete

Outcomes