MPC5604E FEC & fNET

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5604E FEC & fNET

828 Views
suhass
Contributor II

Hi,

I'm working on MPC5604E, using its Fast Ethernet Controller[FEC], & trying to initialize FNET stack on it, but according to "FNET Embedded TCP/IP Stack ", MPC5604E is not supported. [Refer the Image below]

 175080_175080.PNGfnet.PNG

Thanks & Regards

SUHAS S

Labels (1)
0 Kudos
2 Replies

611 Views
martin_kovar
NXP Employee
NXP Employee

Hello Suhas,

From my point of view FNET stack can be used with MPC5604E, but author does not support FNET for the listed platforms anymore as Patrice mentioned above.

Regards,

Martin

0 Kudos

611 Views
Pat
Contributor III

Dear Suhas,

I easily ported fNET on MPC5744P. The MCU dependent files are well identified/organized. Take a look on this thread FNET - Embedded TCP/IP Stack / FNET User Forum / FNET User Forum:Import FNET stack to MPC5748G 

Once the porting completed, you can add/share your files in the fNET. Of course the new one will not be supported even if there is no change. The author can't test fNET on all platforms.

Best regards,

Pat

0 Kudos