Li-Chin Wang

LPCXpresso IDE can't support NGX Xplorer LPC4330 Board with CMSIS-DAP Debugger

Discussion created by Li-Chin Wang on Jan 24, 2017
Latest reply on Jan 24, 2017 by LPCX support

  Customer wants to use LPCXpresso for cost down. I have looked the picture following.

        NGX Xplorer LPC4330 Board only support Redlink. That’s reason why function can’t work fine after I use LINK-II to program code into QSPI      Flash.

        I try to use NXP LPCXpresso4337 to download to NGX Xplorer LPC4330 Board.

        The result is I’m failed to download code to QSPI Flash.

        There is no way for customer to use LPCXpresso IDE and LINK-II right?

        If yes, what’s Redlink debugger and can let customer use LPCXpresso IDE.

        Or customer can only use Keil C to develop LPC4330?

 

 

 

Outcomes