AnsweredAssumed Answered

Are there any pulse de-rating curves for the PESD36VS2UT?

Question asked by Paul Norris on Jan 24, 2017

The datasheet for the PESD36VS2UT does not include a graph to de-rate the power dissipation based on pulse duration but the  PESDxS2UT datasheet does include a graph for the 3V3, 5V2, 12V, 15V and 24V. Can the graph (Fig 4) for the PESD12VS2UT, PESD15VS2UT and PESD24VS2UT be used since these devices are similar power dissipations to the PESD36VS2UT?

Outcomes