According to the specification on NTAG213F, max. Vdd for pullup on FDpin recommended is 3.6V. I am using a battery 3.3-4.2V as supply. Is that a problem?
Regards,
Jesper
Solved! Go to Solution.
Hi Jorge,
Thanks for the clarification. We will add a diode to make sure the voltage will not exceed 3.6V.
Best regards,
Jesper
Hi Jorge,
Thanks for your reply.
I assume you mean keep VDD voltage below 4.6 V - please confirm.
Best regards,
Jesper Selander
Hi Jesper,
Sorry for the confusion. No, I meant keeping the voltage below 3.6 V, as specified in the datasheet:
Regards!
Jorge Gonzalez
Hi Jorge,
Thanks for the clarification. We will add a diode to make sure the voltage will not exceed 3.6V.
Best regards,
Jesper
Hello Jesper Selander,
Actually the limiting value for voltage on the FD pin is 4.6 V. But as stated in the datasheet the exposure to limiting values for extended periods can affect device reliability, see below:
So I highly recommend you to keep VDD voltage below the 3.6 V.
Best Regards!,
Jorge Gonzalez
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------