AnsweredAssumed Answered

SWUpdate for the iMX6

Question asked by 钊 黄 on Jan 22, 2017
Latest reply on Feb 10, 2017 by jimmychan

I am the new user of the Yocto and the i.mx6ull. I follow the guide to add the meta-swupdate layer in the i.mx6ull's BSP. But there is an ERROR in my building process as follow. Can you tell me how to solve this problem? Thanks.

$ bitbake swupdate-image
NOTE: Your conf/bblayers.conf has been automatically updated.
Loading cache: 100% |###########################################| ETA: 00:00:00
Loaded 2796 entries from dependency cache.
Parsing recipes: 100% |#########################################| Time: 00:00:00
Parsing of 2221 .bb files complete (2205 cached, 16 parsed). 2796 targets, 439 skipped, 5 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
Build Configuration:
BB_VERSION = "1.30.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6ull14x14evk"
DISTRO = "fsl-imx-fb"
DISTRO_VERSION = "4.1.15-2.0.0"
TUNE_FEATURES = "arm armv7ve vfp neon callconvention-hard cortexa7"
TARGET_FPU = "hard"
meta
meta-yocto = "HEAD:f5da2a5913319ad6ac2141438ba1aa17576326ab"
meta-oe
meta-multimedia = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-fsl-arm = "HEAD:be78894e4682f111575470fb23e51e6ba523508d"
meta-fsl-arm-extra = "HEAD:3dfb82fc7e703eae9891b3ffda0e9393701f2396"
meta-fsl-demos = "HEAD:a165068f8a0d1cf29aabe4b4053f28be1c2aa492"
meta-bsp
meta-sdk = "HEAD:0451810f7ec7da962bd899f5b0fe26afee1676ca"
meta-browser = "HEAD:77736988073a5d90fcff9d0005c8477332ede387"
meta-gnome
meta-networking
meta-python
meta-filesystems = "HEAD:247b1267bbe95719cd4877d2d3cfbaf2a2f4865a"
meta-qt5 = "HEAD:ccae79be69c5268df3b47e4e14cea0591c39a531"
meta-swupdate = "master:cff58596ed6329c2fd383091fe5fe72ec0ec90ca"
NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: u-boot-fw-utils-v2016.03+gitAUTOINC+df61a74e68-r0 do_compile: oe_runmake failed
ERROR: u-boot-fw-utils-v2016.03+gitAUTOINC+df61a74e68-r0 do_compile: Function failed: do_compile (log file is located at /home/cc/fsl-release-bsp/build-fb-imx6ull14x14evk/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/u-boot-fw-utils/v2016.03+gitAUTOINC+df61a74e68-r0/temp/log.do_compile.36141)
ERROR: Logfile of failure stored in: /home/cc/fsl-release-bsp/build-fb-imx6ull14x14evk/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/u-boot-fw-utils/v2016.03+gitAUTOINC+df61a74e68-r0/temp/log.do_compile.36141
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 4 CROSS_COMPILE=arm-poky-linux-gnueabi- CC=arm-poky-linux-gnueabi-gcc -march=armv7ve -mfpu=neon -mfloat-abi=hard -mcpu=cortex-a7 --sysroot=/home/cc/fsl-release-bsp/build-fb-imx6ull14x14evk/tmp/sysroots/imx6ull14x14evk -O2 -pipe -g -feliminate-unused-debug-types -fdebug-prefix-map=/home/cc/fsl-release-bsp/build-fb-imx6ull14x14evk/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/u-boot-fw-utils/v2016.03+gitAUTOINC+df61a74e68-r0=/usr/src/debug/u-boot-fw-utils/v2016.03+gitAUTOINC+df61a74e68-r0 -fdebug-prefix-map=/home/cc/fsl-release-bsp/build-fb-imx6ull14x14evk/tmp/sysroots/x86_64-linux= -fdebug-prefix-map=/home/cc/fsl-release-bsp/build-fb-imx6ull14x14evk/tmp/sysroots/imx6ull14x14evk= -Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed V=1 mx6ull_14x14_evk_config
| make -f ./scripts/Makefile.build obj=scripts/basic
| rm -f .tmp_quiet_recordmcount
| make -f ./scripts/Makefile.build obj=scripts/kconfig mx6ull_14x14_evk_config
| scripts/kconfig/conf --defconfig=arch/../configs/mx6ull_14x14_evk_defconfig Kconfig
| ***
| *** Can't find default configuration "arch/../configs/mx6ull_14x14_evk_defconfig"!
| ***
| make[1]: *** [mx6ull_14x14_evk_defconfig] Error 1
| make: *** [mx6ull_14x14_evk_config] Error 2
| ERROR: oe_runmake failed
| ERROR: Function failed: do_compile (log file is located at /home/cc/fsl-release-bsp/build-fb-imx6ull14x14evk/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/u-boot-fw-utils/v2016.03+gitAUTOINC+df61a74e68-r0/temp/log.do_compile.36141)
ERROR: Task 818 (/home/cc/fsl-release-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot-fw-utils_2016.03.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1437 tasks of which 1436 didn't need to be rerun and 1 failed.
No currently running tasks (855 of 1482)
Summary: 1 task failed:
/home/cc/fsl-release-bsp/sources/poky/meta/recipes-bsp/u-boot/u-boot-fw-utils_2016.03.bb, do_compile
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

Outcomes