本人是从事人脑脑电采集分析设备开发的,这些设备主要用于科学研究、VR、特殊病情分析等等。目前公司有8通道脑电采集设备,但是采样率比较低,因为MCU KL25频率低,来不及处理。新的一年即将开始了,我希望能领导公司研发人员开发出一款高端的脑电采集设备。
整个系统大致如下图,显示屏主要显示人的情绪指数、注意力指数、电池电量、时间等。AD这边是16通道并行采样,速率是16K次/秒,AD是24位的。数据通过wifi传给PC,PC上有专业的脑电分析软件(公司核心,非本人开发),提取人脑信号回传给LPC54608,MCU发送给需要控制的设备(如假肢,轮椅,玩具等等)。系统通过充电电池供电,可通过USB充电,可连续工作10小时以上。希望通过,非常期待