Camera image stopping issue in IMX356

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Camera image stopping issue in IMX356

651 Views
hyun-moyang
Contributor III

Hi All,

I used IMX356 chipset and video chipset(MAX9526)

In camera preview state, when camera connector is abnormal case, if video chipset(MAX9526) generate the video signal or not  several times, Camera preview image  is stopped in LCD screen in IMX356, or Camera preview image is displayed abnormally in IMX356

please help me to resolve this issue

Tags (1)
0 Kudos
2 Replies

500 Views
hyun-moyang
Contributor III

Hi Igor,

Our BSP Version is Linux-2.6.31 and u-boot.2009.08, and we used the IMX356 chipset.

And Video Chipset of Our Camera is MAX9526,Video Signal is CVBS and BT656.

Regards

HM

0 Kudos

500 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hyun-mo

please try suggestion for implementing new camera driver given in

Chapter 19 Supporting the i.MX53 Camera Sensor Interface CSI0

i.MX53 System Development User’s Guide

http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos