Hi All,
I am trying to play mp4 file of resolution 1080p with imxv4l2sink. It was playing well until i did not install package gstreamer1.0-plugins-imx to the board. Once after installing this package playback is getting stuck after 8 sec.
I am using command gplay-1.0 --video-sink=imxv4l2sink test_1080p.mp4 to play the file.
I tried to find what is creating this issue, and found that if i remove libgstimxcommon.so from /usr/lib then it is working fine.
So i am suspecting that something weird is happening due to libgstimxcommon.so.
How to get rid of this issue ? Any help would be highly appreciated.
My Setup :
fsl-yocto-3.14.28-1.0.0(linux)
board is imx Sabre Auto
Regards,
Hare
Hi Hare,
If you are working with Sabre Auto board, you can try with gst-fsl-plugins described in sect.6.1 Freescale GStreamer plugins:
imxv4l2videosrc is part of community GStreamer-imx plugins supported on meta-fsl-arm mailing list
https://lists.yoctoproject.org/listinfo/meta-freescale
One can post there, so that someone familiar with it could try to assist you.
There are 2 separate plugin's : community GStreamer-imx plugins and
nxp GStreamer Plugins (fsl-gst-plugin package),
Also beside libgstimxcommon.so. Remove the existing plugins
rm /usr/lib/arm-linux-gnueabihf/gstreamer-1.0/libgstimxipu.so
rm /usr/lib/arm-linux-gnueabihf/gstreamer-1.0/libgstimxvpu.so
rm /usr/lib/arm-linux-gnueabihf/gstreamer-1.0/libgstimxeglvivsink.so
rm /usr/lib/libgstimxcommon.so rm /usr/lib/libgstimxcommon.so.0
rm /usr/lib/libgstimxcommon.so.0.9.1
Regards
Hi Bio_TICFSL,
I have two projects. One is using gplay and another one has a pipeline which is using imxvpudec. So i have to keep imxvpudec and its dependent libraries.
Could you tell me why imxvpudec and above mentioned libraries are creating problem ?