Hi Experts,
We are working on iMX6Q sabre AI board. As per the attached Android release notes for i.MX AndroidTM M6.0.1_1.0.0 mentions that for this board GPS connectivity is not applicable but in the attached board schematic diagram interface for GPS module is mentioned.
Our requirement is to use GPS with this board. Please suggest which GPS module (vendor & module part no.) works with iMX6Q sabre AI board & what software changes are required to get GPS module up & running on this board.
Below is the software stack (BSP) I am using
OS:- Android Marshmallow 6.0.1
Kernel:- 3.14.52
U-boot:- 2015.04
Waiting for your reply.
Thanks & Regards,
Vishal Gautam
Hi Vishal
board hardware supports gps uart connection, however no drivers are provided
according to Release Notes. Please check
https://community.nxp.com/message/307613
GpsStatus.NmeaListener | Android Developers
android - How to read GPS data and accelerometer data in one activity - Stack Overflow
geolocation - How do I get the current GPS location programmatically in Android? - Stack Overflow
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------