Hi, Team
Could someone help me the reason why I had a trouble of reading hole with ICODE SLIX2?
We have developed a new Tag with ICODE SLIX2 which showed better read range compared to ICODE SLI.
However, I saw an issue of the reading hole (null point) at the distance close to a reader antenna and as moving
it away from the reader antenna, it is no problem, we can get UID perfectly .
I did not see such a symptom with ICODE SLI.
Best regards,
NA
Hi NA,
This should be a antenna design issue, please kindly check the antenna design on ICODE SLIX2 side, especially the antenna matching. Please refer to the following link for more details.
http://cache.nxp.com/documents/application_note/AN11180.pdf?fsrch=1&sr=1&pageNum=1
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi! Kan
Thank you for your input.
However, this is th case of HF, not UHF which you showed here.
I am afraid that the event is different between two.
Best regards,
NA